Logo
Developing with ZBOSS for Zigbee
zb_zdo_end_device_bind_resp_s Struct Reference

Response from End_Device_Bind_req. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint8_t tsn
 
zb_uint8_t status
 

Detailed Description

Response from End_Device_Bind_req.

See also
ZB spec, subclause 2.4.3.2.1.

Field Documentation

§ status

zb_uint8_t zb_zdo_end_device_bind_resp_s::status

Operation status.

§ tsn

zb_uint8_t zb_zdo_end_device_bind_resp_s::tsn

ZDP transaction sequence number


The documentation for this struct was generated from the following file: