Logo
Developing with ZBOSS for Zigbee

Device unavailable signal parameters. More...

#include <zboss_api_zdo.h>

Data Fields

zb_ieee_addr_t long_addr
 
zb_uint16_t short_addr
 

Detailed Description

Device unavailable signal parameters.

Field Documentation

§ long_addr

zb_ieee_addr_t zb_zdo_device_unavailable_params_s::long_addr

Long address of a device

§ short_addr

zb_uint16_t zb_zdo_device_unavailable_params_s::short_addr

Short address of a device


The documentation for this struct was generated from the following file: