Logo
Developing with ZBOSS for Zigbee
zb_zdo_bind_req_tail_2_s Struct Reference

Bind_req request tail 2nd variant send to the remote. More...

#include <zboss_api_zdo.h>

Data Fields

zb_ieee_addr_t dst_addr
 
zb_uint8_t dst_endp
 

Detailed Description

Bind_req request tail 2nd variant send to the remote.

See also
ZB spec, subclause 2.4.3.2.2.

Field Documentation

§ dst_addr

zb_ieee_addr_t zb_zdo_bind_req_tail_2_s::dst_addr

The destination address for the binding entry.

§ dst_endp

zb_uint8_t zb_zdo_bind_req_tail_2_s::dst_endp

The destination address for the binding entry.


The documentation for this struct was generated from the following file: