Logo
Developing with ZBOSS for Zigbee
zb_zdo_bind_req_param_s Struct Reference

Parameters for Bind_req API call. More...

#include <zboss_api_zdo.h>

Data Fields

zb_ieee_addr_t src_address
 
zb_uint8_t src_endp
 
zb_uint16_t cluster_id
 
zb_uint8_t dst_addr_mode
 
zb_addr_u dst_address
 
zb_uint8_t dst_endp
 
zb_uint16_t req_dst_addr
 

Detailed Description

Parameters for Bind_req API call.

See also
ZB spec, subclause 2.4.3.2.2.

Field Documentation

§ cluster_id

zb_uint16_t zb_zdo_bind_req_param_s::cluster_id

The identifier of the cluster on the source device that is bound to the destination.

§ dst_addr_mode

zb_uint8_t zb_zdo_bind_req_param_s::dst_addr_mode

Destination address mode bind_dst_addr_mode

§ dst_address

zb_addr_u zb_zdo_bind_req_param_s::dst_address

The destination address for the binding entry.

§ dst_endp

zb_uint8_t zb_zdo_bind_req_param_s::dst_endp

This field shall be present only if the DstAddrMode field has a value of ZB_BIND_DST_ADDR_MODE_64_BIT_EXTENDED bind_dst_addr_mode and, if present, shall be the destination endpoint for the binding entry.

§ req_dst_addr

zb_uint16_t zb_zdo_bind_req_param_s::req_dst_addr

Destination address of the request

§ src_address

zb_ieee_addr_t zb_zdo_bind_req_param_s::src_address

The IEEE address for the source.

§ src_endp

zb_uint8_t zb_zdo_bind_req_param_s::src_endp

The source endpoint for the binding entry.


The documentation for this struct was generated from the following file: