#include <zb_zcl_tunneling.h>
Data Fields | |
| zb_uint8_t | protocol_list_complete |
| zb_uint8_t | protocol_count |
| zb_zcl_tunneling_protocol_field_t | protocol_list [16] |
SupportedTunnelProtocolResponse command payload.
| zb_uint8_t zb_zcl_tunneling_supported_tunnel_protocols_response_s::protocol_count |
The number of Protocol fields contained in the response.
| zb_zcl_tunneling_protocol_field_t zb_zcl_tunneling_supported_tunnel_protocols_response_s::protocol_list[16] |
The payload of the response should be capable of holding up to 16 protocols.
| zb_uint8_t zb_zcl_tunneling_supported_tunnel_protocols_response_s::protocol_list_complete |
The Protocol List Complete field is a Boolean; a value of 0(ZB_FALSE) indicates that there are more supported protocols available (if more than 16 protocols are supported). A value of 1(ZB_TRUE) indicates that the list of supported protocols is complete.