RequestTunnelResponse command payload More...
#include <zb_zcl_tunneling.h>
Data Fields | |
| zb_uint16_t | tunnel_id |
| A number between 0..65535 that uniquely identifies the tunnel that has been allocated in the server triggered through the RequestTunnel command. This ID must now be used to send data through this tunnel (TunnelID, TransferData) and is also required to close the tunnel again (CloseTunnel). If the command has failed, the TunnelStatus contains the reason of the error and the TunnelID is set to 0xFFFF. | |
| zb_uint8_t | tunnel_status |
| The TunnelStatus parameter indicates the server’s internal status after the execution of a RequestTunnel command. More... | |
| zb_uint16_t | max_incoming_transfer_size |
| A value that defines the size, in octets, of the maximum data packet that can be transferred to the server in the payload of a single TransferData command. | |
RequestTunnelResponse command payload
| zb_uint8_t zb_zcl_tunneling_request_tunnel_response_s::tunnel_status |
The TunnelStatus parameter indicates the server’s internal status after the execution of a RequestTunnel command.