#include <zb_zcl_tunneling.h>
Data Fields | |
| zb_uint16_t | tunnel_id |
| zb_uint16_t | number_of_octets_left |
ReadyData command payload
| zb_uint16_t zb_zcl_tunneling_ready_data_s::number_of_octets_left |
Indicates the number of octets that may be received by the initiator of this command (receiver). It is most likely the remaining size of the buffer holding the data that is sent over TransferData.
| zb_uint16_t zb_zcl_tunneling_ready_data_s::tunnel_id |
A number between 0..65535 that uniquely identifies the tunnel that has been allocated in the server triggered through the RequestTunnel command.