#include <zb_zcl_tunneling.h>
Data Fields | |
| zb_uint16_t | manufacturer_code |
| zb_uint8_t | protocol_id |
Supported Tunnel Protocols Response Command Protocol Fields
| zb_uint16_t zb_zcl_tunneling_protocol_field_s::manufacturer_code |
A code that is allocated by the Zigbee Alliance, relating the manufacturer to a device and - for tunneling - a manufacturer specific protocol.
| zb_uint8_t zb_zcl_tunneling_protocol_field_s::protocol_id |
An enumeration representing the identifier of the metering communication protocol for the supported tunnel.