#include <zb_zcl_tunneling.h>
Data Fields | |
| zb_uint8_t | protocol_offset |
GetSupportedTunnelProtocols command payload
| zb_uint8_t zb_zcl_tunneling_get_supported_tunnel_protocols_s::protocol_offset |
Where there are more protocols supported than can be returned in a single Supported TunnelProtocolsResponse command, this field allows an offset to be specified on subsequent GetSupportedTunnelProtocols commands