CloseTunnel command payload More...
#include <zb_zcl_tunneling.h>
Data Fields | |
| zb_uint16_t | tunnel_id |
| The identifier of the tunnel that shall be closed. It is the same number that has been previously returned in the response to a RequestTunnel command. Valid numbers range between 0..65535 and must correspond to a tunnel that is still active and maintained by the server. | |
CloseTunnel command payload