Logo
Developing with ZBOSS for Zigbee
zb_zcl_sub_ghz_attrs_s Struct Reference

Sub GHz cluster attributes. More...

#include <zb_zcl_subghz.h>

Data Fields

zb_uint32_t channel_change
 
zb_uint32_t page28_channel_mask
 
zb_uint32_t page29_channel_mask
 
zb_uint32_t page30_channel_mask
 
zb_uint32_t page31_channel_mask
 

Detailed Description

Sub GHz cluster attributes.

Field Documentation

§ channel_change

zb_uint32_t zb_zcl_sub_ghz_attrs_s::channel_change

§ page28_channel_mask

zb_uint32_t zb_zcl_sub_ghz_attrs_s::page28_channel_mask

§ page29_channel_mask

zb_uint32_t zb_zcl_sub_ghz_attrs_s::page29_channel_mask

§ page30_channel_mask

zb_uint32_t zb_zcl_sub_ghz_attrs_s::page30_channel_mask

§ page31_channel_mask

zb_uint32_t zb_zcl_sub_ghz_attrs_s::page31_channel_mask

The documentation for this struct was generated from the following file: