Logo
Developing with ZBOSS for Zigbee
zb_zcl_scenes_recall_scene_transition_time_req_s Struct Reference

Recall scene command transition_time payload structure. More...

#include <zb_zcl_scenes.h>

Data Fields

zb_uint16_t transition_time
 

Detailed Description

Recall scene command transition_time payload structure.

Field Documentation

§ transition_time

zb_uint16_t zb_zcl_scenes_recall_scene_transition_time_req_s::transition_time

Determines how long the transition takes from the old cluster state to the new cluster state


The documentation for this struct was generated from the following file: