#include <zb_zcl_commands.h>
Data Fields | |
| zb_uint8_t | status |
| zb_uint8_t | direction |
| zb_uint16_t | attr_id |
| union { | |
| struct { | |
| zb_uint8_t attr_type | |
| zb_uint16_t min_interval | |
| zb_uint16_t max_interval | |
| zb_uint8_t delta [1] | |
| } clnt | |
| struct { | |
| zb_uint16_t timeout | |
| } srv | |
| } | u |
Format of the Attribute Reporting Configuration Record Field Figure 2.22 in ZCL spec. NOTE: it can be various number of attribute recording configuration record fields in Read reporting configuration response
| zb_uint16_t zb_zcl_read_reporting_cfg_rsp_s::attr_id |
The attribute identifier field is 16 bits in length and shall contain the identifier of the attribute that the reporting configuration details apply to
| zb_uint8_t zb_zcl_read_reporting_cfg_rsp_s::attr_type |
Attribute data type
| struct { ... } zb_zcl_read_reporting_cfg_rsp_s::clnt |
clnt: if the direction field is set to 0, then the attribute data type field, the minimum reporting interval field, the maximum reporting interval field and the reportable change field are included in the payload, and the timeoutperiod field is omitted.
| zb_uint8_t zb_zcl_read_reporting_cfg_rsp_s::delta[1] |
The reportable change field shall contain the minimum change to the attribute that will result in a report being issued. For attributes with 'analog' data type (see Table 2.16) the field has the same data type as the attribute. If the reportable change has not been configured, this field shall contain the invalid value for the relevant data type. For attributes of 'discrete' data type (see Table 2.16) this field is omitted.
| zb_uint8_t zb_zcl_read_reporting_cfg_rsp_s::direction |
The direction field specifies whether values of the attribute are reported (0x00), or whether reports of the attribute are received (0x01).
| zb_uint16_t zb_zcl_read_reporting_cfg_rsp_s::max_interval |
The maximum reporting interval field is 16 bits in length and shall contain the maximum interval, in seconds, between issuing reports for the attribute specified in the attribute identifier field. If the maximum reporting interval has not been configured, this field shall contain the value 0xffff.
| zb_uint16_t zb_zcl_read_reporting_cfg_rsp_s::min_interval |
The minimum reporting interval field is 16 bits in length and shall contain the minimum interval, in seconds, between issuing reports for the attribute specified in the attribute identifier field. If the minimum reporting interval has not been configured, this field shall contain the value 0xffff.
| struct { ... } zb_zcl_read_reporting_cfg_rsp_s::srv |
srv: if the direction field is set to 1, then the timeout period field is included in the payload, and the attribute data type field, the minimum reporting interval field, the maximum reporting interval field and the reportable change field are omitted.
| zb_uint8_t zb_zcl_read_reporting_cfg_rsp_s::status |
If the attribute is not implemented on the sender or receiver of the command, whichever is relevant (depending on direction), this field shall be set to UNSUPPORTED_ATTRIBUTE. If the attribute is supported, but is not capable of being reported, this field shall be set to UNREPORTABLE_ATTRIBUTE. Otherwise, this field shall be set to SUCCESS.
| zb_uint16_t zb_zcl_read_reporting_cfg_rsp_s::timeout |
The timeout period field is 16 bits in length and shall contain the maximum expected time, in seconds, between received reports for the attribute specified in the attribute identifier field. If the timeout period has not been configured, this field shall contain the value 0xffff.
| union { ... } zb_zcl_read_reporting_cfg_rsp_s::u |
Response contents: different for client and server