#include <zb_zcl_price.h>
Data Fields | |
| zb_uint32_t | earliest_start_time |
| zb_uint32_t | min_issuer_event_id |
| zb_uint8_t | number_of_commands |
| zb_uint8_t | tariff_type |
GetTariffInformation command payload
| zb_uint32_t zb_zcl_price_get_tariff_information_payload_s::earliest_start_time |
UTC Timestamp indicating the earliest start time of tariffs to be returned by the corresponding PublishTariffInformation command.
| zb_uint32_t zb_zcl_price_get_tariff_information_payload_s::min_issuer_event_id |
A 32-bit integer representing the minimum IssuerEventID of tariffs to be returned by the corresponding PublishTariffInformation command.
| zb_uint8_t zb_zcl_price_get_tariff_information_payload_s::number_of_commands |
An 8-bit integer which represents the maximum number of PublishTariffInformation commands that the client is willing to receive in response to this command. A value of 0 would indicate all available PublishTariffInformation commands shall be returned.
| zb_uint8_t zb_zcl_price_get_tariff_information_payload_s::tariff_type |
An 8-bit bitmap identifying the type of tariff published in this command. The least significant nibble represents an enumeration of the tariff type. The most significant nibble is reserved