Logo
Developing with ZBOSS for Zigbee
zb_zcl_price_get_price_matrix_payload_s Struct Reference

#include <zb_zcl_price.h>

Data Fields

zb_uint32_t issuer_tariff_id
 

Detailed Description

GetPriceMatrix command payload

See also
SE spec, subclause D.4.2.3.9

Field Documentation

§ issuer_tariff_id

zb_uint32_t zb_zcl_price_get_price_matrix_payload_s::issuer_tariff_id

IssuerTariffID indicates the tariff to which the requested Price Matrix belongs.


The documentation for this struct was generated from the following file: