Logo
Developing with ZBOSS for Zigbee
zb_zcl_price_get_current_price_payload_s Struct Reference

GetCurrentPrice Command Payload Format More...

#include <zb_zcl_price.h>

Data Fields

zb_uint8_t command_options
 

Detailed Description

GetCurrentPrice Command Payload Format

Field Documentation

§ command_options

zb_uint8_t zb_zcl_price_get_current_price_payload_s::command_options

CommandOptions field is 8 Bits in length

Note
Zero bit is Requestor Rx On When Idle, others are reserved.

The documentation for this struct was generated from the following file: