#include <zb_zcl_price.h>
Data Fields | |
| zb_uint32_t | earliest_start_time |
| zb_uint32_t | min_issuer_event_id |
| zb_uint8_t | number_of_commands |
| zb_uint8_t | tariff_type |
GetConsolidatedBill command payload
| zb_uint32_t zb_zcl_price_get_consolidated_bill_payload_s::earliest_start_time |
UTC Timestamp indicating the earliest start time of billing information to be returned by the corresponding PublishConsolidatedBill command.
| zb_uint32_t zb_zcl_price_get_consolidated_bill_payload_s::min_issuer_event_id |
A 32-bit integer representing the minimum IssuerEventID of billing information to be returned by the corresponding PublishConsolidatedBill command.
| zb_uint8_t zb_zcl_price_get_consolidated_bill_payload_s::number_of_commands |
An 8-bit Integer which indicates the maximum number of PublishConsolidatedBill commands that can be sent. A value of 0 would indicate all available PublishConsolidatedBill commands shall be returned.
| zb_uint8_t zb_zcl_price_get_consolidated_bill_payload_s::tariff_type |
An 8-bit bitmap identifying the TariffType of the requested BillingPeriod information. The least significant nibble represents an enumeration of the tariff type. The most significant nibble is reserved.