Logo
Developing with ZBOSS for Zigbee
zb_zcl_prepayment_set_overall_debt_cap_payload_s Struct Reference

#include <zb_zcl_prepayment.h>

Data Fields

zb_uint32_t provider_id
 
zb_uint32_t issuer_event_id
 
zb_uint32_t implementation_date
 
zb_int32_t overall_debt_cap
 

Detailed Description

Set Overall Debt Cap Payload

See also
SE spec, subclause D.7.2.3.13

Field Documentation

§ implementation_date

zb_uint32_t zb_zcl_prepayment_set_overall_debt_cap_payload_s::implementation_date

A UTC Time field to indicate the date from which the overall debt cap is to be applied. An Implementation Date/Time of 0x00000000 shall indicate that the command should be executed immediately.

§ issuer_event_id

zb_uint32_t zb_zcl_prepayment_set_overall_debt_cap_payload_s::issuer_event_id

Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.

§ overall_debt_cap

zb_int32_t zb_zcl_prepayment_set_overall_debt_cap_payload_s::overall_debt_cap

A signed 32-bit integer that defines the total amount of debt that can be taken from top-ups. This field is always a monetary value, and as such the field is measured in a base unit of Currency with the decimal point.

§ provider_id

zb_uint32_t zb_zcl_prepayment_set_overall_debt_cap_payload_s::provider_id

An unsigned 32-bit field containing a unique identifier for the commodity supplier to whom this command relates.


The documentation for this struct was generated from the following file: