#include <zb_zcl_prepayment.h>
Data Fields | |
| zb_uint8_t | command_index |
| zb_uint8_t | commands_total_number |
| zb_zcl_prepayment_debt_payload_record_t * | debt_payload |
Publish Debt Log Command Payload
| zb_uint8_t zb_zcl_prepayment_publish_debt_log_payload_s::command_index |
An UTC time field identifying the time when the collection occurred.
| zb_uint8_t zb_zcl_prepayment_publish_debt_log_payload_s::commands_total_number |
An unsigned 32-bit field to denote the amount of debt collected at this time.
| zb_zcl_prepayment_debt_payload_record_t* zb_zcl_prepayment_publish_debt_log_payload_s::debt_payload |
The Debt Payload shall contain one or more debt records zb_zcl_prepayment_debt_payload_record_t