#include <zb_zcl_prepayment.h>
Data Fields | |
| zb_uint8_t | friendly_credit |
| zb_uint32_t | friendly_credit_calendar_id |
| zb_uint32_t | emergency_credit_limit |
| zb_uint32_t | emergency_credit_threshold |
Change Payment Mode Response Command Payload
| zb_uint32_t zb_zcl_prepayment_payment_mode_response_payload_s::emergency_credit_limit |
An unsigned 32-bit field to denote the emergency credit limit on the Metering Device, measured in base unit of Currency with the decimal point located as indicated by the TrailingDigits field, as defined in the Price cluster.
| zb_uint32_t zb_zcl_prepayment_payment_mode_response_payload_s::emergency_credit_threshold |
An unsigned 32-bit field to denote the amount of credit remaining on the Metering Device below which the Emergency Credit facility can be selected. The value is measured in base unit of Currency with the decimal point located as indicated by the TrailingDigits field, as defined in the Price cluster.
| zb_uint8_t zb_zcl_prepayment_payment_mode_response_payload_s::friendly_credit |
An 8-bit BitMap to show if the meter has a Friendly Credit calendar and that this calendar shall be enabled.
| zb_uint32_t zb_zcl_prepayment_payment_mode_response_payload_s::friendly_credit_calendar_id |
An unsigned 32-bit field to denote the IssuerCalendarID that shall be used for the friendly credit periods