#include <zb_zcl_prepayment.h>
Data Fields | |
| zb_uint32_t | latest_end_time |
| zb_uint8_t | records_number |
Get Top Up Log Payload
| zb_uint32_t zb_zcl_prepayment_get_top_up_log_payload_s::latest_end_time |
UTC timestamp indicating the latest TopUp Time of Top Up records to be returned by the corresponding Publish Top Up Log commands.
| zb_uint8_t zb_zcl_prepayment_get_top_up_log_payload_s::records_number |
An 8-bit integer which represents the maximum number of records that the client is willing to receive in response to this command. A value of 0 would indicate all available records shall be returned.