Logo
Developing with ZBOSS for Zigbee
zb_zcl_prepayment_get_prepay_snapshot_payload_s Struct Reference

#include <zb_zcl_prepayment.h>

Data Fields

zb_uint32_t earliest_start_time
 
zb_uint32_t latest_end_time
 
zb_uint8_t snapshot_offset
 
zb_uint32_t snapshot_cause
 

Detailed Description

Get Prepay Snapshot Command Payload

See also
SE spec, subclause D.7.2.3.8

Field Documentation

§ earliest_start_time

zb_uint32_t zb_zcl_prepayment_get_prepay_snapshot_payload_s::earliest_start_time

A UTC Timestamp indicating the earliest time of a snapshot to be returned by a corresponding Publish Prepay Snapshot command.

§ latest_end_time

zb_uint32_t zb_zcl_prepayment_get_prepay_snapshot_payload_s::latest_end_time

A UTC Timestamp indicating the latest time of a snapshot to be returned by a corresponding Publish Prepay Snapshot command.

§ snapshot_cause

zb_uint32_t zb_zcl_prepayment_get_prepay_snapshot_payload_s::snapshot_cause

This field is used to request only snapshots for a specific cause.

§ snapshot_offset

zb_uint8_t zb_zcl_prepayment_get_prepay_snapshot_payload_s::snapshot_offset

Where multiple snapshots satisfy the selection criteria specified by the other fields in this command, this field identifies the individual snapshot to be returned.


The documentation for this struct was generated from the following file: