#include <zb_zcl_prepayment.h>
Data Fields | |
| zb_uint32_t | issuer_event_id |
| zb_uint32_t | start_time |
| zb_uint32_t | emergency_credit_limit |
| zb_uint32_t | emergency_credit_threshold |
Emergency Credit Setup Command Payload
| zb_uint32_t zb_zcl_prepayment_emergency_credit_setup_payload_s::emergency_credit_limit |
An unsigned 32-bit field to denote the Emergency Credit limit on the Metering Device, measured in base unit of Currency or in Units with the decimal point.
| zb_uint32_t zb_zcl_prepayment_emergency_credit_setup_payload_s::emergency_credit_threshold |
An unsigned 32-bit field to denote the amount of credit remaining on the Metering Device below which the Emergency Credit facility can be selected. The value is measured in base unit of Currency or in Units with the decimal points.
| zb_uint32_t zb_zcl_prepayment_emergency_credit_setup_payload_s::issuer_event_id |
Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.
| zb_uint32_t zb_zcl_prepayment_emergency_credit_setup_payload_s::start_time |
A UTC Time field to denote the time at which the Emergency Credit settings become valid. A start date/time of 0x00000000 shall indicate that the command should be executed immediately.