#include <zb_zcl_prepayment.h>
Change Debt Command Payload
| zb_int32_t zb_zcl_prepayment_change_debt_command_payload_s::debt_amount |
The format and use of this field is the same as for the DebtAmount::N attribute as defined in D.7.2.2.3.2.
| zb_uint8_t zb_zcl_prepayment_change_debt_command_payload_s::debt_amount_type |
An 8-bit enumeration field identifying the type of debt information to be issued within this command.
| zb_uint8_t zb_zcl_prepayment_change_debt_command_payload_s::debt_label[13] |
The format and use of this field is the same as for the DebtLabel::N attribute as defined in D.7.2.2.3.1.
| zb_int32_t zb_zcl_prepayment_change_debt_command_payload_s::debt_recovery_amount |
The format and use of this field is the same as for the DebtRecoveryAmount::N attribute as defined in D.7.2.2.3.7.
| zb_uint16_t zb_zcl_prepayment_change_debt_command_payload_s::debt_recovery_balance_percentage |
The format and use of this field is the same as for the DebtRecoveryTopUpPercentage::N attribute as defined in D.7.2.2.3.8.
| zb_uint16_t zb_zcl_prepayment_change_debt_command_payload_s::debt_recovery_collection_time |
The format and use of this field is the same as for the DebtRecoveryCollectionTime::N attribute as defined in D.7.2.2.3.5.
| zb_uint8_t zb_zcl_prepayment_change_debt_command_payload_s::debt_recovery_frequency |
The format and use of this field is the same as for the DebtRecoveryFrequency::N attribute as defined in D.7.2.2.3.6.
| zb_uint8_t zb_zcl_prepayment_change_debt_command_payload_s::debt_recovery_method |
The format and use of this field is the same as for the DebtRecoveryMethod::N attribute as defined in D.7.2.2.3.3.
| zb_uint32_t zb_zcl_prepayment_change_debt_command_payload_s::debt_recovery_start_time |
The format and use of this field is the same as for the DebtRecoveryStartTime::N attribute as defined in D.7.2.2.3.4.
| zb_uint32_t zb_zcl_prepayment_change_debt_command_payload_s::issuer_event_id |
Unique identifier generated by the commodity provider. When new information is provided that replaces older information for the same time period, this field allows devices to determine which information is newer.