Logo
Developing with ZBOSS for Zigbee
zb_zcl_poll_control_check_in_res_s Struct Reference

Structure representation of Check-in response command payload. More...

#include <zb_zcl_poll_control.h>

Data Fields

zb_uint8_t is_start
 
zb_uint16_t timeout
 

Detailed Description

Structure representation of Check-in response command payload.

Field Documentation

§ is_start

zb_uint8_t zb_zcl_poll_control_check_in_res_s::is_start

Start Fast Polling

§ timeout

zb_uint16_t zb_zcl_poll_control_check_in_res_s::timeout

Fast Poll Timeout


The documentation for this struct was generated from the following file: