Logo
Developing with ZBOSS for Zigbee
zb_zcl_poll_control_check_in_cli_param_s Struct Reference

Parameters to pass to device callback for incoming check in. More...

#include <zb_zcl_poll_control.h>

Data Fields

zb_uint16_t fast_poll_timeout
 
zb_uint16_t short_addr
 
zb_uint8_t ep
 

Detailed Description

Parameters to pass to device callback for incoming check in.


The documentation for this struct was generated from the following file: