Logo
Developing with ZBOSS for Zigbee
zb_zcl_ota_upgrade_sub_element_s Struct Reference

Structure representation of OTA File Sub-element, see ZCL8 specification, subsection 11.4.3. More...

#include <zb_zcl_ota_upgrade.h>

Data Fields

zb_uint16_t tag_id
 
zb_uint32_t length
 
zb_uint8_t value [1]
 

Detailed Description

Structure representation of OTA File Sub-element, see ZCL8 specification, subsection 11.4.3.

Field Documentation

§ length

zb_uint32_t zb_zcl_ota_upgrade_sub_element_s::length

Tag ID

§ value

zb_uint8_t zb_zcl_ota_upgrade_sub_element_s::value[1]

length


The documentation for this struct was generated from the following file: