Logo
Developing with ZBOSS for Zigbee
zb_zcl_ota_upgrade_image_block_s Struct Reference

Structure representation of Image Block Request command payload. More...

#include <zb_zcl_ota_upgrade.h>

Data Fields

zb_uint8_t fc
 
zb_uint16_t manufacturer
 
zb_uint16_t image_type
 
zb_uint32_t file_version
 
zb_uint32_t file_offset
 
zb_uint8_t data_size_max
 
zb_ieee_addr_t node_addr
 
zb_uint16_t block_delay
 

Detailed Description

Structure representation of Image Block Request command payload.

See also
ZCL8 specification, subsection 11.13.6.1

Field Documentation

§ block_delay

zb_uint16_t zb_zcl_ota_upgrade_image_block_s::block_delay

BlockRequestDelay

§ data_size_max

zb_uint8_t zb_zcl_ota_upgrade_image_block_s::data_size_max

Maximum data size

§ fc

zb_uint8_t zb_zcl_ota_upgrade_image_block_s::fc

§ file_offset

zb_uint32_t zb_zcl_ota_upgrade_image_block_s::file_offset

File offset

§ file_version

zb_uint32_t zb_zcl_ota_upgrade_image_block_s::file_version

File version

§ image_type

zb_uint16_t zb_zcl_ota_upgrade_image_block_s::image_type

Image type

§ manufacturer

zb_uint16_t zb_zcl_ota_upgrade_image_block_s::manufacturer

Manufacturer code

§ node_addr

zb_ieee_addr_t zb_zcl_ota_upgrade_image_block_s::node_addr

Request node address


The documentation for this struct was generated from the following file: