#include <zb_zcl_metering.h>
Data Fields | |
| zb_uint8_t | applied_update_period_in_seconds |
| zb_uint32_t | fast_poll_mode_end_time |
RequestFastPollModeResponse command payload
| zb_uint8_t zb_zcl_metering_request_fast_poll_mode_response_payload_s::applied_update_period_in_seconds |
The period at which metering data shall be updated. This may be different than the requested fast poll.
| zb_uint32_t zb_zcl_metering_request_fast_poll_mode_response_payload_s::fast_poll_mode_end_time |
UTC time that indicates when the metering server will terminate fast poll mode and resume updating at the rate specified by DefaultUpdatePeriod.