#include <zb_zcl_metering.h>
Data Fields | |
| zb_uint16_t | sample_id |
| zb_uint32_t | earliest_sample_time |
| zb_uint8_t | sample_type |
| zb_uint16_t | number_of_samples |
GetSampledData command payload
| zb_uint32_t zb_zcl_metering_get_sampled_data_payload_s::earliest_sample_time |
A UTC Timestamp indicating the earliest time of a sample to be returned.
| zb_uint16_t zb_zcl_metering_get_sampled_data_payload_s::number_of_samples |
Represents the number of samples being requested, This value cannot exceed the size stipulated in the MaxNumberOfSamples field in the StartSampling command.
| zb_uint16_t zb_zcl_metering_get_sampled_data_payload_s::sample_id |
Unique identifier allocated to this Sampling session. This field allows devices to match response data with the appropriate request.
| zb_uint8_t zb_zcl_metering_get_sampled_data_payload_s::sample_type |
An 8-bit enumeration that identifies the type of data being sampled.