Logo
Developing with ZBOSS for Zigbee
zb_zcl_metering_get_profile_response_payload_s Struct Reference

#include <zb_zcl_metering.h>

Data Fields

zb_uint32_t end_time
 
zb_uint8_t status
 
zb_uint8_t profile_interval_period
 
zb_uint8_t number_of_periods_delivered
 
zb_uint24_t * intervals
 

Detailed Description

GetProfileResponse command payload

See also
SE spec, subclause D.3.2.3.1.1.1

Field Documentation

§ end_time

zb_uint32_t zb_zcl_metering_get_profile_response_payload_s::end_time

It is 32-bit value (in UTC) representing the end time of the most chronologically recent interval being requested.

§ intervals

zb_uint24_t* zb_zcl_metering_get_profile_response_payload_s::intervals

Series of interval data captured using the period specified by the ProfileIntervalPeriod field. The content of the interval data depends of the type of information requested using the Channel field in the GetProfileCommand, and will represent the change in that information since the previous interval.

§ number_of_periods_delivered

zb_uint8_t zb_zcl_metering_get_profile_response_payload_s::number_of_periods_delivered

Represents the number of intervals the device is returning.

§ profile_interval_period

zb_uint8_t zb_zcl_metering_get_profile_response_payload_s::profile_interval_period

Represents the interval or time frame used to capture metered Energy, Gas, and Water consumption for profiling purposes.

See also
zb_zcl_metering_profile_interval_period_e

§ status

zb_uint8_t zb_zcl_metering_get_profile_response_payload_s::status

The documentation for this struct was generated from the following file: