Logo
Developing with ZBOSS for Zigbee
zb_zcl_messaging_display_message_payload_s Struct Reference

#include <zb_zcl_messaging.h>

Data Fields

zb_uint32_t message_id
 
zb_uint8_t message_control
 
zb_uint32_t start_time
 
zb_uint16_t duration_in_minutes
 
zb_uint8_t message_len
 
zb_uint8_tmessage
 
zb_uint8_t extended_message_control
 

Detailed Description

DisplayMessage command payload

See also
SE spec, subclause D.5.2.3.1.1

Field Documentation

§ duration_in_minutes

zb_uint16_t zb_zcl_messaging_display_message_payload_s::duration_in_minutes

The amount of time in minutes after the Start Time during which the message is displayed

§ extended_message_control

zb_uint8_t zb_zcl_messaging_display_message_payload_s::extended_message_control

BitMap field indicating additional control and status information for a given message.

§ message_control

zb_uint8_t zb_zcl_messaging_display_message_payload_s::message_control

BitMap field indicating control information related to the message

§ message_id

zb_uint32_t zb_zcl_messaging_display_message_payload_s::message_id

32-bit number identifier for the message.

§ message_len

zb_uint8_t zb_zcl_messaging_display_message_payload_s::message_len

Message (variable): Character String WARNING: Variable length of message supported, but remember to pass strings in global memory only!

§ start_time

zb_uint32_t zb_zcl_messaging_display_message_payload_s::start_time

The time at which the message becomes valid


The documentation for this struct was generated from the following file: