Logo
Developing with ZBOSS for Zigbee
zb_zcl_keep_alive_attrs_s Struct Reference

Keep-Alive cluster attributes. More...

#include <zb_zcl_keep_alive.h>

Data Fields

zb_uint8_t base
 TC Keep-Alive Base attribute. More...
 
zb_uint16_t jitter
 TC Keep-Alive Jitter attribute. More...
 

Detailed Description

Keep-Alive cluster attributes.

Field Documentation

§ base

zb_uint8_t zb_zcl_keep_alive_attrs_s::base

TC Keep-Alive Base attribute.

See also
ZB_ZCL_ATTR_KEEP_ALIVE_TC_KEEP_ALIVE_BASE_ID

§ jitter

zb_uint16_t zb_zcl_keep_alive_attrs_s::jitter

TC Keep-Alive Jitter attribute.

See also
ZB_ZCL_ATTR_KEEP_ALIVE_TC_KEEP_ALIVE_JITTER_ID

The documentation for this struct was generated from the following file: