Structure is used to pass parameters for ZoneStatus notification command. More...
#include <zb_zcl_ias_zone.h>
Data Fields | |
| zb_uint8_t | ep |
| zb_uint16_t | status_val |
| zb_uint16_t | delay |
Structure is used to pass parameters for ZoneStatus notification command.
| zb_uint16_t zb_zcl_ias_zone_notification_param_s::delay |
Delay
| zb_uint8_t zb_zcl_ias_zone_notification_param_s::ep |
endpoint number
| zb_uint16_t zb_zcl_ias_zone_notification_param_s::status_val |
new value of zone_zone_status, see zb_zcl_ias_zone_zonestatus_e