Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_zone_enroll_res_s Struct Reference

Structure representsation of Enroll response command payload see ZCL spec 8.2.2.3.1.1. More...

#include <zb_zcl_ias_zone.h>

Data Fields

zb_uint8_t code
 
zb_uint8_t zone_id
 

Detailed Description

Structure representsation of Enroll response command payload see ZCL spec 8.2.2.3.1.1.

Field Documentation

§ code

zb_uint8_t zb_zcl_ias_zone_enroll_res_s::code

Enroll response code

§ zone_id

zb_uint8_t zb_zcl_ias_zone_enroll_res_s::zone_id

Zone ID


The documentation for this struct was generated from the following file: