Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_wd_squawk_s Struct Reference

Structure representsation Squawk command. ZCL spec 8.4.2.3.2. More...

#include <zb_zcl_ias_wd.h>

Data Fields

zb_uint8_t status
 

Detailed Description

Structure representsation Squawk command. ZCL spec 8.4.2.3.2.

Field Documentation

§ status

zb_uint8_t zb_zcl_ias_wd_squawk_s::status

Status - enum flags Squawk mode, Strobe and Squawk level, see ZCL spec 8.4.2.3.2


The documentation for this struct was generated from the following file: