Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_ace_get_zone_id_map_resp_s Struct Reference

Structure representsation of Get Zone ID Map Response command, ZCL spec 8.3.2.5.2.1. More...

#include <zb_zcl_ias_ace.h>

Data Fields

zb_uint16_t zone_id_map [ZB_ZCL_IAS_ACE_GET_ZONE_ID_MAP_LENGTH]
 

Detailed Description

Structure representsation of Get Zone ID Map Response command, ZCL spec 8.3.2.5.2.1.

Field Documentation

§ zone_id_map

zb_uint16_t zb_zcl_ias_ace_get_zone_id_map_resp_s::zone_id_map[ZB_ZCL_IAS_ACE_GET_ZONE_ID_MAP_LENGTH]

Zone ID Map


The documentation for this struct was generated from the following file: