Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_ace_bypass_resp_s Struct Reference

Structure representsation of Bypass Response command, ZCL spec 8.3.2.4.8. More...

#include <zb_zcl_ias_ace.h>

Data Fields

zb_uint8_t length
 
zb_uint8_t bypass_result [ZB_ZCL_IAS_ACE_ZONE_TABLE_LENGTH]
 

Detailed Description

Structure representsation of Bypass Response command, ZCL spec 8.3.2.4.8.

Field Documentation

§ bypass_result

zb_uint8_t zb_zcl_ias_ace_bypass_resp_s::bypass_result[ZB_ZCL_IAS_ACE_ZONE_TABLE_LENGTH]

Bypass Result for Zone IDs, see zb_zcl_ias_ace_bypass_result_e

§ length

zb_uint8_t zb_zcl_ias_ace_bypass_resp_s::length

Number of Zones


The documentation for this struct was generated from the following file: