Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_ace_arm_s Struct Reference

Structure representsation of Arm command, ZCL spec 8.3.2.4.1.1. More...

#include <zb_zcl_ias_ace.h>

Data Fields

zb_uint8_t arm_mode
 
zb_uchar_t arm_disarm_code [ZB_ZCL_MAX_STRING_SIZE]
 
zb_uint8_t zone_id
 

Detailed Description

Structure representsation of Arm command, ZCL spec 8.3.2.4.1.1.

Field Documentation

§ arm_disarm_code

zb_uchar_t zb_zcl_ias_ace_arm_s::arm_disarm_code[ZB_ZCL_MAX_STRING_SIZE]

Arm/Disarm Code

§ arm_mode

zb_uint8_t zb_zcl_ias_ace_arm_s::arm_mode

§ zone_id

zb_uint8_t zb_zcl_ias_ace_arm_s::zone_id

Zone ID


The documentation for this struct was generated from the following file: