Logo
Developing with ZBOSS for Zigbee
zb_zcl_ias_ace_arm_resp_s Struct Reference

Structure representation of Arm Response command, ZCL spec 8.3.2.5.1. More...

#include <zb_zcl_ias_ace.h>

Data Fields

zb_uint8_t arm_notification
 

Detailed Description

Structure representation of Arm Response command, ZCL spec 8.3.2.5.1.

Field Documentation

§ arm_notification

zb_uint8_t zb_zcl_ias_ace_arm_resp_s::arm_notification

Arm Notification, see zb_zcl_ias_ace_arm_not_e


The documentation for this struct was generated from the following file: