Logo
Developing with ZBOSS for Zigbee
zb_zcl_go_to_tilt_percentage_req_s Struct Reference

Structured representation of GO_TO_TILT_PERCENTAGE command payload. More...

#include <zb_zcl_window_covering.h>

Data Fields

zb_uint8_t percentage_tilt_value
 

Detailed Description

Structured representation of GO_TO_TILT_PERCENTAGE command payload.

See also
ZCL8 spec, subclause 7.4.2.2.7.1

Field Documentation

§ percentage_tilt_value

zb_uint8_t zb_zcl_go_to_tilt_percentage_req_s::percentage_tilt_value

Percentage Tilt Value


The documentation for this struct was generated from the following file: