#include <zb_zcl_events.h>
Data Fields | |
| zb_uint8_t | log_id |
| zb_uint16_t | event_id |
| zb_uint32_t | event_time |
| zb_uint8_t | event_control |
| zb_uint8_t | event_data [44] |
PublishEvent Command payload
| zb_uint8_t zb_zcl_events_publish_event_payload_s::event_control |
An 8-bit bitmap specifying actions to be taken regarding particular event.
| zb_uint8_t zb_zcl_events_publish_event_payload_s::event_data[44] |
A variable length octet string array used to hold additional information captured when the event occurred. The first element (element 0) of the array indicates the length of the string, NOT including the first element.
| zb_uint16_t zb_zcl_events_publish_event_payload_s::event_id |
The Event ID specifies a particular event
| zb_uint32_t zb_zcl_events_publish_event_payload_s::event_time |
The timestamp of the event occurrence in UTC format.
| zb_uint8_t zb_zcl_events_publish_event_payload_s::log_id |
The least significant nibble is an enumeration indicating the Log ID. The most significant nibble is reserved.