Logo
Developing with ZBOSS for Zigbee
zb_zcl_events_clear_event_log_response_s Struct Reference

#include <zb_zcl_events.h>

Data Fields

zb_uint8_t cleared_events_logs
 

Detailed Description

ClearEventLogResponse command payload

See also
SE spec, D.11.2.4.3

Field Documentation

§ cleared_events_logs

zb_uint8_t zb_zcl_events_clear_event_log_response_s::cleared_events_logs

This 8-bit Bitmask indicates which logs have been cleared.

See also
SE spec, Table D-191 and zb_zcl_events_cleared_events_logs_bitmap_t

The documentation for this struct was generated from the following file: