Logo
Developing with ZBOSS for Zigbee
zb_zcl_events_clear_event_log_request_s Struct Reference

#include <zb_zcl_events.h>

Data Fields

zb_uint8_t log_id
 

Detailed Description

ClearEventLogRequest command payload

See also
SE spec, subclause D.11.2.3.2

Field Documentation

§ log_id

zb_uint8_t zb_zcl_events_clear_event_log_request_s::log_id

The least significant nibble specifies the Log to be cleared. The most significant nibble is reserved.


The documentation for this struct was generated from the following file: