#include <zb_zcl_energy_mgmt.h>
Data Fields | |
| zb_uint32_t | issuer_event_id |
| zb_uint16_t | device_class |
| zb_uint8_t | utility_enrollment_group |
| zb_uint8_t | actions_required |
ManageEvent command Payload
| zb_uint8_t zb_zcl_energy_management_manage_event_payload_s::actions_required |
Bit encoded field indicating the action(s) to be carried out in regard to the associated event
| zb_uint16_t zb_zcl_energy_management_manage_event_payload_s::device_class |
Bit encoded field representing the DRLC client Device Class to apply the current Load Control Event. Each bit, if set individually or in combination, indicates the class of device(s) the Manage Event command is directed at.
| zb_uint32_t zb_zcl_energy_management_manage_event_payload_s::issuer_event_id |
Unique identifier generated by the Energy provider. The value of this field allows the command to be matched with a specific Load Control Event.
| zb_uint8_t zb_zcl_energy_management_manage_event_payload_s::utility_enrollment_group |
The DRLC client Utility Enrollment Group field can be used in conjunction with the Device Class bits. It provides a mechanism to direct the Manage Event command to groups of devices.