#include <zb_zcl_drlc.h>
Data Fields | |
| zb_uint32_t | start_time |
| zb_uint8_t | number_of_events |
| zb_uint32_t | issuer_event_id |
GetScheduledEvents command payload
| zb_uint32_t zb_zcl_drlc_get_scheduled_events_payload_s::issuer_event_id |
Represents the minimum Issuer Event ID of events to be matched and sent by the server with the same Start Time as the Get Scheduled Events command. A value of 0xFFFFFFFF indicates this field will not be used.
| zb_uint8_t zb_zcl_drlc_get_scheduled_events_payload_s::number_of_events |
Represents the maximum number of events to be sent. A value of 0 indicates no maximum limit.
| zb_uint32_t zb_zcl_drlc_get_scheduled_events_payload_s::start_time |
UTC Timestamp representing the minimum Start Time of events that shall be matched and sent by the Server. A Start Time of 0x00000000 has no special meaning.