Logo
Developing with ZBOSS for Zigbee

#include <zb_zcl_drlc.h>

Data Fields

zb_uint32_t issuer_event_id
 
zb_uint16_t device_class
 
zb_uint8_t utility_enrollment_group
 
zb_uint8_t cancel_control
 
zb_uint32_t effective_time
 

Detailed Description

CancelLoadControlEvent command payload

See also
SE spec, Figure D-3

Field Documentation

§ cancel_control

zb_uint8_t zb_zcl_drlc_cancel_lce_payload_s::cancel_control

This field is used to indicate that the Event is currently in process and a cancel command is received.

§ device_class

zb_uint16_t zb_zcl_drlc_cancel_lce_payload_s::device_class

Bit encoded field representing the Device Class to apply the current Load Control Event. Each bit, if set individually or in combination, indicates the class device(s) needing to participate in the event.

§ effective_time

zb_uint32_t zb_zcl_drlc_cancel_lce_payload_s::effective_time

UTC Timestamp representing when the canceling of the event is scheduled to start. An effective time of 0x00000000 is a special time denoting “now.”

§ issuer_event_id

zb_uint32_t zb_zcl_drlc_cancel_lce_payload_s::issuer_event_id

Unique identifier generated by the Energy provider. The value of this field allows matching of Event reports with a specific Demand Response and Load Control event.

§ utility_enrollment_group

zb_uint8_t zb_zcl_drlc_cancel_lce_payload_s::utility_enrollment_group

This field can be used in conjunction with the Device Class bits for providing a mechanism to direct Load Control Events to groups of Devices.


The documentation for this struct was generated from the following file: