#include <zb_zcl_drlc.h>
Data Fields | |
| zb_uint8_t | cancel_control |
CancelAllLoadControlEvents command payload
| zb_uint8_t zb_zcl_drlc_cancel_alce_payload_s::cancel_control |
Where the Cancel Control field indicates that randomization is to be used, the receiving device should first check whether Duration Time was to be randomized and, if so, termination of the event should be adjusted according to the value of the DurationRandomizationMinutes attribute.