Logo
Developing with ZBOSS for Zigbee

ZCL Discover Attribute Command frame. More...

#include <zb_zcl_commands.h>

Data Fields

zb_uint16_t start_attr_id
 
zb_uint8_t maximum
 

Detailed Description

ZCL Discover Attribute Command frame.

See also
ZCL spec, zb_zcl_disc_attr 2.4.13 Discover Attributes Command

Field Documentation

§ maximum

zb_uint8_t zb_zcl_disc_attr_req_s::maximum

Maximum attribute identifiers

§ start_attr_id

zb_uint16_t zb_zcl_disc_attr_req_s::start_attr_id

Start attribute identifier


The documentation for this struct was generated from the following file: