UpdateSiteID Command Payload Format More...
#include <zb_zcl_device_management.h>
Data Fields | |
| zb_uint32_t | issuer_event_id |
| zb_uint32_t | site_id_time |
| zb_uint32_t | provider_id |
| zb_uint32_t | site_id [ZB_ZCL_DEVICE_MANAGEMENT_SITE_ID_MAX_SIZE] |
UpdateSiteID Command Payload Format
| zb_uint32_t zb_zcl_device_management_update_site_id_cmd_payload_s::issuer_event_id |
The Issuer Event ID field represents a unique identifier generated by the commodity provider.
| zb_uint32_t zb_zcl_device_management_update_site_id_cmd_payload_s::provider_id |
The Provider ID field represents a unique identifier for the commodity provider to whom this command relates.
| zb_uint32_t zb_zcl_device_management_update_site_id_cmd_payload_s::site_id[ZB_ZCL_DEVICE_MANAGEMENT_SITE_ID_MAX_SIZE] |
The Site ID field represents the Site ID (see max size below).
| zb_uint32_t zb_zcl_device_management_update_site_id_cmd_payload_s::site_id_time |
The SiteID Time field represents a UTC time at which the update of SiteID will take place.